AXIS#.MOTOR.VOLTMIN
Description
This parameter configures the drive for the induction motor's minimum voltage at standstill. It is given as a percentage (%) of the motor’s rated voltage. AXIS#.MOTOR.VOLTMIN is used to calculate the constant volts per Hertz characteristics of the drive and motor and should be set to a value that generates a current of about 40% of the rated current at standstill.
Context
For more information see Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
% |
|
Range |
0 to 100 |
|
Default Value |
2 |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.MOTOR.VOLTMIN |
500bh |
07h |
Unsigned16 |
- |
- |
Read/Write |
No |
|
AXIS2.MOTOR.VOLTMIN |
510bh |
07h |
Unsigned16 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
6225 |
1 |
6225 (0x1851) |
AXIS1.MOTOR.VOLTMIN |
Unsigned16 |
Read/Write |
Yes |
|
71761 |
2 |
6225 (0x1851) |
AXIS2.MOTOR.VOLTMIN |
Unsigned16 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.MOTOR.VOLTMIN |
6225 |
Unsigned16 |
Read/Write |
- |