AXIS#.MT.P

Description

Specifies the motion task position. Depending on the motion task control word (AXIS#.MT.CNTL), the AXIS#.MT.P command can either be the target position of the motion task or a relative distance.

Examples

Code

Sets the position of motion task 0 to 360 degrees. The first parameter is the motion task number and the second is the position.

-->AXIS1.MT.P 0 360

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only Array

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

0

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MT.P 0

50d6h

01h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 1

50d6h

02h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 2

50d6h

03h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 3

50d6h

04h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 4

50d6h

05h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 5

50d6h

06h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 6

50d6h

07h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 7

50d6h

08h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 8

50d6h

09h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 9

50d6h

0ah

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 10

50d6h

0bh

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 11

50d6h

0ch

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 12

50d6h

0dh

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 13

50d6h

0eh

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 14

50d6h

0fh

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 15

50d6h

10h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 16

50d6h

11h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 17

50d6h

12h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 18

50d6h

13h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 19

50d6h

14h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 20

50d6h

15h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 21

50d6h

16h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 22

50d6h

17h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 23

50d6h

18h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 24

50d6h

19h

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 25

50d6h

1ah

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 26

50d6h

1bh

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 27

50d6h

1ch

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 28

50d6h

1dh

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 29

50d6h

1eh

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 30

50d6h

1fh

Signed32

Position

-

Read/Write

No

AXIS1.MT.P 31

50d6h

20h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 0

51d6h

01h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 1

51d6h

02h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 2

51d6h

03h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 3

51d6h

04h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 4

51d6h

05h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 5

51d6h

06h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 6

51d6h

07h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 7

51d6h

08h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 8

51d6h

09h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 9

51d6h

0ah

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 10

51d6h

0bh

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 11

51d6h

0ch

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 12

51d6h

0dh

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 13

51d6h

0eh

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 14

51d6h

0fh

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 15

51d6h

10h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 16

51d6h

11h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 17

51d6h

12h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 18

51d6h

13h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 19

51d6h

14h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 20

51d6h

15h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 21

51d6h

16h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 22

51d6h

17h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 23

51d6h

18h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 24

51d6h

19h

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 25

51d6h

1ah

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 26

51d6h

1bh

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 27

51d6h

1ch

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 28

51d6h

1dh

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 29

51d6h

1eh

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 30

51d6h

1fh

Signed32

Position

-

Read/Write

No

AXIS2.MT.P 31

51d6h

20h

Signed32

Position

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6307

1

6307 (0x18a3)

AXIS1.MT.P

Signed32[32]

Read/Write

Yes

71843

2

6307 (0x18a3)

AXIS2.MT.P

Signed32[32]

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MT.P

6307

Signed32[32]

Read/Write

Position

Related Topics

Motion Tasks