AXIS#.PROFINET.GEARRATIO.SHAFTREV

Description

The count of driving shaft revolutions for the position gear ratio calculation used for PROFINET position units.

See Units.

Versions

Action Version Notes
Implemented 02-04-02-000  

General Information

Type Read/Write
Units

N/A

Range 1 to 4294967295
Default Value 1
Data Type Integer
Stored in Non Volatile Memory Yes

Variants Supported

PROFINET drives: AKD2G-SPP