AXIS#.SENSORLESS.FAULTTIME
Description
Sets the maximum time allowed for the commutation angle error estimated by Sensorless Field-Oriented Control (SFOC) to be above AXIS#.SENSORLESS.FAULTANGLE before faulting. Adjust this value as needed for your application.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-03-03-000 |
|
General Information
|
Type |
Read/Write |
| Description | Sets the minimum fault detection time for SFOC |
|
Units |
ms |
| Range | 1 to 10000 |
| Default Value | 10 |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.SENSORLESS.FAULTTIME |
5018h |
04h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
AXIS2.SENSORLESS.FAULTTIME |
5118h |
04h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
7403 |
1 |
7403 (0x1ceb) |
AXIS1.SENSORLESS.FAULTTIME |
Signed32 |
Read/Write |
Yes |
|
72939 |
2 |
7403 (0x1ceb) |
AXIS2.SENSORLESS.FAULTTIME |
Signed32 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.SENSORLESS.FAULTTIME |
7403 |
Float |
Read/Write |
- |