AXIS#.SENSORLESS.ISTART

Description

Sensorless Field-Oriented Control (SFOC) runs in open-loop when velocity is below a certain limit and automatically switches to closed loop when velocity goes above that limit. This limit is determined by AXIS#.SENSORLESS​.RPMSTART. There is a hysteresis band to make the transition seamless.

At open-loop, a constant current is applied to the motor to accelerate and reach AXIS#.SENSORLESS.RPMSTART. This constant current is determined by AXIS#.SENSORLESS.ISTART.


  • In the open-loop mode, AXIS#.SENSORLESS.ISTART value determines the maximum torque rather than the actual torque. The actual torque that is applied can be anywhere between 0 and this maximum torque depending on the load.

Versions

Action Version Notes
Implemented 02-03-03-000

 

General Information

Type

Read/Write

Description Sets the starting current for SFOC

Units

Arms

Range

0 to Drive’s Peak Current

Default Value

5% of Drive’s Peak Current

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SENSORLESS.ISTART

5018h

05h

Signed32

-

1000:1

Read/Write

No

AXIS2.SENSORLESS.ISTART

5118h

05h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

7405

1

7405 (0x1ced)

AXIS1.SENSORLESS.ISTART

Signed32

Read/Write

Yes

72941

2

7405 (0x1ced)

AXIS2.SENSORLESS.ISTART

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.SENSORLESS.ISTART

7405

Float

Read/Write

-