AXIS#.TUNING.BANDWIDTH

Description

AXIS#.TUNING.BANDWIDTH can be used to determine what the bandwidth of the velocity loop is. The motor inertia, load inertia and velocity loop proportional gains are all considered in this calculation.

Note:

This keyword will only return a valid value if AXIS#.TUNING.ISSLIDERINUSE is True (1). Complex tuning solutions that include various filters invalidate the use of this.

The value displayed in the Slider Tuning View is linked to this value.

Versions

Action Version Notes
Implemented 02-13-01-000 

-

General Information

Type Read Only
Units Hz
Range 0.0 to 300.0 Hz 
Default Value 0.0
Data Type Double
See Also

AXIS#.VL.KP

AXIS#.MOTOR.INERTIA

AXIS#.LOAD.INERTIA

AXIS#.TUNING.ISSLIDERINUSE

Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.TUNING.BANDWIDTH

5021h

01h

Signed32

-

1000:1

Read/Write

No

AXIS2.TUNING.BANDWIDTH

5121h

01h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5040

1

5040 (0x13b0)

AXIS1.TUNING.BANDWIDTH

Signed32

Read/Write

Yes

70576

2

5040 (0x13b0)

AXIS2.TUNING.BANDWIDTH

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.TUNING.BANDWIDTH

5040

Float

Read/Write

-