AXIS#.TUNING.DEFAULT

Description

AXIS#.TUNING.DEFAULT resets all tuning parameters to their defaults and tunes the axis to achieve 75Hz Velocity Loop bandwidth assuming a 1:1 Motor to load Inertia ratio.

Default tuning is calculated using AXIS#.MOTOR.KT , AXIS#.MOTOR.INERTIA , and AXIS#.MOTOR.LQLL .

Example

The following will reset all tuning parameters to their default and tune the axis.

-->AXIS1.TUNING.DEFAULT
-->

Versions

Action Version Notes
Implemented 02-14-01-000 

-

General Information

Type Action
Units N/A
Range N/A
Default Value N/A
Data Type N/A
Stored in Non-Volatile Memory N/A

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.TUNING.DEFAULT

5021h

02h

Unsigned32

-

-

Write only

No

AXIS2.TUNING.DEFAULT

5121h

02h

Unsigned32

-

-

Write only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5046

1

5046 (0x13b6)

AXIS1.TUNING.DEFAULT

Unsigned8

Read/Write

No

70582

2

5046 (0x13b6)

AXIS2.TUNING.DEFAULT

Unsigned8

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.TUNING.DEFAULT

5046

Unsigned8

Read/Write

-