AXIS#.VL.FF

Description

This parameter displays the velocity loop overall feedforward value.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

0 to AXIS#.VL.LIMITP

Default Value

0

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.VL.FF

5011h

2ch

Signed32

-

1000:1

Read only

No

AXIS2.VL.FF

5111h

2ch

Signed32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6027

1

6027 (0x178b)

AXIS1.VL.FF

Signed32

Read Only

Yes

71563

2

6027 (0x178b)

AXIS2.VL.FF

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.FF

6027

Float

Read Only

Velocity

Related Topics

"Velocity Loop"

AXIS#.VL.KVFF