AXIS#.VL.KFB

Description

AXIS#.VL.KFB allows the user to scale the velocity feedback source into the velocity control loops

This is especially useful in dual-loop applications where the position loop feedback and velocity loop feedback come from different devices. AXIS#.PL.KFB and AXIS#.VL.KFB can be used to synchronize the values.

Examples

Usage

By default AXIS#.VL.KFB is set to 1.0 and should not be set to another value unless the application is using multiple feedback devices for a axis.

If the situation arose where two feedbacks were mounted to a rotary motor, and one of them was half the resolution of the first - and it was connected to the position feedback, while the full resolution device was connected to the velocity feedback, AXIS#.PL.KFB would need to be set to 2.0 and AXIS#.VL.KFB would be left at 1.0.

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type Read/Write
Units N/A
Range Double
Default Value 1
Data Type Float
See Also AXIS#.PL.KFB
Stored in Non-Volatile Memory Yes

Variants Supported

Supported on all device types.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.VL.KFB

5011h

23h

Signed32

-

1000:1

Read/Write

No

AXIS2.VL.KFB

5111h

23h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6046

1

6046 (0x179e)

AXIS1.VL.KFB

Signed32

Read/Write

Yes

71582

2

6046 (0x179e)

AXIS2.VL.KFB

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.KFB

6046

Float

Read/Write

-