AXIS#.WS.NUMLOOPS

Description

This parameter sets the maximum number of wake and shake repetitions. AXIS#.MOTOR.PHASE is calculated as mean value of all wake and shake repetitions.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

counts

Range

0 to 20 counts

Default Value

5 counts

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.WS.NUMLOOPS

5013h

02h

Unsigned8

-

-

Read/Write

No

AXIS2.WS.NUMLOOPS

5113h

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6705

1

6705 (0x1a31)

AXIS1.WS.NUMLOOPS

Unsigned8

Read/Write

Yes

72241

2

6705 (0x1a31)

AXIS2.WS.NUMLOOPS

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.WS.NUMLOOPS

6705

Unsigned8

Read/Write

-