AXIS#.CLRWARNINGS

Description

AXIS#.CLRWARNINGS tries to clear all active warnings on the axis.

Each axis has several warnings that stay set after motion is commanded.

These are not cleared until:

These warnings include W6000 and W6004.

Many warnings are continuously monitored and AXIS#.CLRWARNINGS will not clear these. These can only be cleared by removing the generating condition or possibly by changing a related parameter. For example, warning 2007 "bus under voltage" the bus voltage can be increased or change VBUS.UVWTHRESH.

See Faults and Warning Messages for details regarding the behavior of individual faults.

Versions

Action Version Notes
Implemented 02-05-01-000

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5034

1

5034 (0x13aa)

AXIS1.CLRWARNINGS

Unsigned8

Read/Write

No

70570

2

5034 (0x13aa)

AXIS2.CLRWARNINGS

Unsigned8

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.CLRWARNINGS

5034

Unsigned8

Read/Write

-

Related Topics

AXIS#.CLRFAULTS, DRV.CLRFAULTS, AXIS#.EN , AXIS#.DIS