AXIS#.DBILIMIT
Description
This parameter sets the maximum amplitude of the current for dynamic braking. AXIS#.DBILIMIT can only be set manually when AXIS#.MOTOR.DISAUTOSET index (28) is set to 1. Setting AXIS#.MOTOR.AUTOSET to 0 does not make AXIS#.DBILIMIT writeable.
-
- If the motor or drive current is in foldback before entering dynamic brake mode, the actual current limit might be less than AXIS#.DBILIMIT when dynamic braking starts. The current will be limited to the minimum of AXIS#.DBILIMIT and AXIS#.IL.IFOLD . Once the foldback current recovers, AXIS#.DBILIMIT will be the enforced current limit.
Example
Setting AXIS#.DBILIMIT to 2 limits the dynamic brake current to 2 Arms.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
| Bug fix | 02-08-00-000 | The bug caused AXIS#.DBILIMIT to be reset to its default value under some conditions. The fix involved making the parameter read only by default and calculated from motor parameters. |
General Information
|
Type |
Read/Write |
|
Units |
Arms |
|
Range |
0 to minimum of drive peak current (IPEAK) and motor peak current (AXIS#.MOTOR.IPEAK ). |
|
Default Value |
Drive continuous current (ICONT) |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.DBILIMIT |
5000h |
07h |
Unsigned32 |
- |
1000:1 |
Read/Write |
No |
|
AXIS2.DBILIMIT |
5100h |
07h |
Unsigned32 |
- |
1000:1 |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5005 |
1 |
5005 (0x138d) |
AXIS1.DBILIMIT |
Unsigned32 |
Read Only |
Yes |
|
70541 |
2 |
5005 (0x138d) |
AXIS2.DBILIMIT |
Unsigned32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.DBILIMIT |
5005 |
Float |
Read Only |
- |