AXIS#.FAULTSCUSTOMCFG

Description

This keyword is used to configure the mapping used by AXIS#.FAULTSCUSTOM. Each entry is a comma separated list of up to 13 drive fault numbers that are mapped to the custom fault code equal to the entry’s index. The fault numbers may contain ‘x’ as a wildcard. Faults that are not explicitly mapped to any fault code are implicitly mapped to code 255.

Examples

Map one fault (F5000 - Motor overheated) to fault code 1

AXIS1.FAULTSCUSTOMCFG 1 5000

Map multiple faults (F2006 and F2007 – Bus over and under voltage) to fault code 2

AXIS1.FAULTSCUSTOMCFG 2 2006,2007

Map multiple faults using wildcards (F41xx – All feedback 1 faults) to fault code 3

AXIS1.FAULTSCUSTOMCFG 3 41xx

Versions

Action Version Notes
Implemented 02-15-01-000  

General Information

Type Read Only
Units N/A
Range N/A
Index Range 1 to 254
Default Value Empty
Data Type String

Stored in Non-Volatile Memory

Yes

Variants Supported

Supported on all device types.