AXIS#.FAULTSCUSTOMCYCLE
Description
This keyword configures the interval at which AXIS#.FAULTSCUSTOM cycles through fault codes.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-15-01-000 |
General Information
| Type | Read/Write |
| Units | Milliseconds |
| Range | 500 to 10000 |
| Default Value | 4000 |
| Data Type | Integer |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
Supported on all device types.