AXIS#.FAULT#

Description

This keyword can be used to extract individual faults from the axis specified.

The order of the faults are represented by the order of the faults thrown.


  • Only the fault number is returned, no detail description is accompanied.

Examples

If there were two faults present on Axis1, they could be extracted using AXIS1.FAULT1 and AXIS1.FAULT2 seen below:

-->AXIS1.FAULT1
4312
-->AXIS1.FAULT2
4115

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type Read Only
Units N/A
Range N/A
Default Value N/A
Data Type Integer
See Also AXIS#.FAULTS, DRV.FAULTS

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.FAULT1

5004h

01h

Unsigned16

-

-

Read only

No

AXIS1.FAULT2

5004h

02h

Unsigned16

-

-

Read only

No

AXIS1.FAULT3

5004h

03h

Unsigned16

-

-

Read only

No

AXIS1.FAULT4

5004h

04h

Unsigned16

-

-

Read only

No

AXIS1.FAULT5

5004h

05h

Unsigned16

-

-

Read only

No

AXIS1.FAULT6

5004h

06h

Unsigned16

-

-

Read only

No

AXIS1.FAULT7

5004h

07h

Unsigned16

-

-

Read only

No

AXIS1.FAULT8

5004h

08h

Unsigned16

-

-

Read only

No

AXIS1.FAULT9

5004h

09h

Unsigned16

-

-

Read only

No

AXIS1.FAULT10

5004h

0ah

Unsigned16

-

-

Read only

No

AXIS2.FAULT1

5104h

01h

Unsigned16

-

-

Read only

No

AXIS2.FAULT2

5104h

02h

Unsigned16

-

-

Read only

No

AXIS2.FAULT3

5104h

03h

Unsigned16

-

-

Read only

No

AXIS2.FAULT4

5104h

04h

Unsigned16

-

-

Read only

No

AXIS2.FAULT5

5104h

05h

Unsigned16

-

-

Read only

No

AXIS2.FAULT6

5104h

06h

Unsigned16

-

-

Read only

No

AXIS2.FAULT7

5104h

07h

Unsigned16

-

-

Read only

No

AXIS2.FAULT8

5104h

08h

Unsigned16

-

-

Read only

No

AXIS2.FAULT9

5104h

09h

Unsigned16

-

-

Read only

No

AXIS2.FAULT10

5104h

0ah

Unsigned16

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6800

1

6800 (0x1a90)

AXIS1.FAULT1

Unsigned16

Read Only

Yes

72336

2

6800 (0x1a90)

AXIS2.FAULT1

Unsigned16

Read Only

Yes

6801

1

6801 (0x1a91)

AXIS1.FAULT2

Unsigned16

Read Only

Yes

72337

2

6801 (0x1a91)

AXIS2.FAULT2

Unsigned16

Read Only

Yes

6802

1

6802 (0x1a92)

AXIS1.FAULT3

Unsigned16

Read Only

Yes

72338

2

6802 (0x1a92)

AXIS2.FAULT3

Unsigned16

Read Only

Yes

6803

1

6803 (0x1a93)

AXIS1.FAULT4

Unsigned16

Read Only

Yes

72339

2

6803 (0x1a93)

AXIS2.FAULT4

Unsigned16

Read Only

Yes

6804

1

6804 (0x1a94)

AXIS1.FAULT5

Unsigned16

Read Only

Yes

72340

2

6804 (0x1a94)

AXIS2.FAULT5

Unsigned16

Read Only

Yes

6805

1

6805 (0x1a95)

AXIS1.FAULT6

Unsigned16

Read Only

Yes

72341

2

6805 (0x1a95)

AXIS2.FAULT6

Unsigned16

Read Only

Yes

6806

1

6806 (0x1a96)

AXIS1.FAULT7

Unsigned16

Read Only

Yes

72342

2

6806 (0x1a96)

AXIS2.FAULT7

Unsigned16

Read Only

Yes

6807

1

6807 (0x1a97)

AXIS1.FAULT8

Unsigned16

Read Only

Yes

72343

2

6807 (0x1a97)

AXIS2.FAULT8

Unsigned16

Read Only

Yes

6808

1

6808 (0x1a98)

AXIS1.FAULT9

Unsigned16

Read Only

Yes

72344

2

6808 (0x1a98)

AXIS2.FAULT9

Unsigned16

Read Only

Yes

6809

1

6809 (0x1a99)

AXIS1.FAULT10

Unsigned16

Read Only

Yes

72345

2

6809 (0x1a99)

AXIS2.FAULT10

Unsigned16

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.FAULT1

6800

Unsigned16

Read Only

-

AXIS#.FAULT2

6801

Unsigned16

Read Only

-

AXIS#.FAULT3

6802

Unsigned16

Read Only

-

AXIS#.FAULT4

6803

Unsigned16

Read Only

-

AXIS#.FAULT5

6804

Unsigned16

Read Only

-

AXIS#.FAULT6

6805

Unsigned16

Read Only

-

AXIS#.FAULT7

6806

Unsigned16

Read Only

-

AXIS#.FAULT8

6807

Unsigned16

Read Only

-

AXIS#.FAULT9

6808

Unsigned16

Read Only

-

AXIS#.FAULT10

6809

Unsigned16

Read Only

-