AXIS#.ICONT

Description

AXIS#.ICONT returns the drive continuous rated current in Arms.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Arms

Range

N/A

Default Value

N/A

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.ICONT

5000h

0bh

Signed32

-

1000:1

Read only

No

AXIS2.ICONT

5100h

0bh

Signed32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5013

1

5013 (0x1395)

AXIS1.ICONT

Signed32

Read Only

Yes

70549

2

5013 (0x1395)

AXIS2.ICONT

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.ICONT

5013

Float

Read Only

-