AXIS#.NAME
Description
This parameter is used to set the name of the axis.
Code
-->AXIS1.NAME Axis 1 -->AXIS2.NAME Axis 2 -->AXIS1.NAME Axis 1 -->AXIS2.NAME Axis 2
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
Axis1 for AXIS1 and Axis 2 for AXIS2 |
|
Data Type |
String |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.NAME |
5000h |
01h |
String(32) |
- |
- |
Read/Write |
No |
|
AXIS2.NAME |
5100h |
01h |
String(32) |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5000 |
1 |
5000 (0x1388) |
AXIS1.NAME |
String |
Read/Write |
No |
|
70536 |
2 |
5000 (0x1388) |
AXIS2.NAME |
String |
Read/Write |
No |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.NAME |
5000 |
String |
Read/Write |
- |