AXIS#.UTWTHRESH
Description
This parameter returns the under temperature warning threshold of the power circuit for the specified axis. The value depends on the drive model. It is programmed in the drive and cannot be changed.
General Information
|
Type |
Read Only |
|
Units |
degC |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Float |
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.UTWTHRESH |
5000h |
17h |
Signed32 |
- |
- |
Read only |
No |
|
AXIS2.UTWTHRESH |
5100h |
17h |
Signed32 |
- |
- |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5030 |
1 |
5030 (0x13a6) |
AXIS1.UTWTHRESH |
Signed32 |
Read Only |
Yes |
|
70566 |
2 |
5030 (0x13a6) |
AXIS2.UTWTHRESH |
Signed32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.UTWTHRESH |
5030 |
Float |
Read Only |
- |