AXIS#.ZEROV

Description

AXIS#.ZEROV is the velocity threshold for the motor to be considered at zero velocity.

Versions

Action Version Notes
Implemented 02-00-00-000

 

Renamed from AXIS#.DISVTHRESH 02-03-00-000  

General Information

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

Linear: counts/s, mm/s, µm/s, (custom units)/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

5 RPM

Depends on units. See Velocity Units for details.

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.ZEROV

5002h

04h

Signed32

Velocity

-

Read/Write

No

AXIS2.ZEROV

5102h

04h

Signed32

Velocity

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5002

1

5002 (0x138a)

AXIS1.ZEROV

Signed32

Read/Write

Yes

70538

2

5002 (0x138a)

AXIS2.ZEROV

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.ZEROV

5002

Float

Read/Write

Velocity