BRAKE#.AXIS

Description

Sets which axis will control the brake.

Value Description
0 Not used
1 Controlled by Axis 1
2 Controlled by Axis 2

Examples

Context

For more information see Brake.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 2

Default Value

Depends on Brake and Axis number:

BRAKE1 defaults to 1.

BRAKE2 defaults to 2 on multi-axis drives and 0 on single-axis drives.

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

BRAKE1.AXIS

3012h

01h

Unsigned8

-

-

Read/Write

No

BRAKE2.AXIS

3012h

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

3100

1

3100 (0xc1c)

BRAKE1.AXIS

Unsigned8

Read/Write

Yes

3101

1

3101 (0xc1d)

BRAKE2.AXIS

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

BRAKE1.AXIS

3100

Unsigned8

Read/Write

-

BRAKE2.AXIS

3101

Unsigned8

Read/Write

-