CAP#.ARM

Description

Arms or disarms the capture channel.

The capture channel needs to be armed to start the process of monitoring the trigger input and sampling the source on the selected edge. Setting CAP#.ARM to zero will stop the capture process.

After each capture event, CAP#.ARM is reset to 0 and must be armed again by setting CAP#.ARM to 1, before another value can be captured. If CAP#.REARM is 1 or 2 then CAP#.ARM stays at 1 and keeps capturing new values until CAP#.ARM is set to zero.

Examples

Usage

0: Disabled (default)

1: Armed

Code

-->CAP1.ARM 1
-->

Context

See Capture.

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type Read/Write
Units N/A
Range

0 to 1

Default Value 0
Data Type Integer
See Also CAP#.REARM
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

CAP1.ARM

4400h

09h

Unsigned8

-

-

Read/Write

No

CAP2.ARM

4401h

09h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

31000

1

31000 (0x7918)

CAP1.ARM

Unsigned8

Read/Write

Yes

31001

1

31001 (0x7919)

CAP2.ARM

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

CAP1.ARM

31000

Unsigned8

Read/Write

-

CAP2.ARM

31001

Unsigned8

Read/Write

-