DIO#.DIR

Description

Sets or whether the bi-directional IO is an input or output.

Value Description
0 The bi-directional IO is treated as an input signal
1 The bi-directional IO is treated as an output signal

Examples

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0 (input)
Data Type Integer
See Also  

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

DIO1.DIR

368ah

01h

Unsigned8

-

-

Read/Write

No

DIO2.DIR

368bh

01h

Unsigned8

-

-

Read/Write

No

DIO3.DIR

368ch

01h

Unsigned8

-

-

Read/Write

No

DIO4.DIR

368dh

01h

Unsigned8

-

-

Read/Write

No

DIO5.DIR

368eh

01h

Unsigned8

-

-

Read/Write

No

DIO6.DIR

368fh

01h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

22050

1

22050 (0x5622)

DIO1.DIR

Unsigned8

Read/Write

Yes

22051

1

22051 (0x5623)

DIO2.DIR

Unsigned8

Read/Write

Yes

22052

1

22052 (0x5624)

DIO3.DIR

Unsigned8

Read/Write

Yes

22053

1

22053 (0x5625)

DIO4.DIR

Unsigned8

Read/Write

Yes

22054

1

22054 (0x5626)

DIO5.DIR

Unsigned8

Read/Write

Yes

22055

1

22055 (0x5627)

DIO6.DIR

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

DIO1.DIR

22050

Unsigned8

Read/Write

-

DIO2.DIR

22051

Unsigned8

Read/Write

-

DIO3.DIR

22052

Unsigned8

Read/Write

-

DIO4.DIR

22053

Unsigned8

Read/Write

-

DIO5.DIR

22054

Unsigned8

Read/Write

-

DIO6.DIR

22055

Unsigned8

Read/Write

-