DOUT.STATES

Description

DOUT.STATES reads the states of the digital outputs. Each bit corresponds to a digital state. Bit 0 = DOUT1 ... Bit 8 = DOUT9.

Examples

Usage

When DOUT1 and DOUT3 are active (DOUT#.STATE = 1). Bits 0 and 2 would be set. DOUT.STATES would be 5.

Code

--> DOUT.STATES
5

Context

See Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

 

General Information

Type Read Only
Units N/A
Range 0 to 511
Default Value N/A
Data Type Integer
See Also  

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

DOUT.STATES

3600h

00h

Unsigned32

-

-

Read only

Yes

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2702

1

2702 (0xa8e)

DOUT.STATES

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

DOUT.STATES

2702

Unsigned32

Read Only

-