DOUT#.STATEU
Description
Gets or sets the user command state of the specified digital output when DOUT#.SOURCE = 0 (user).
| Value | Description |
|---|---|
| 0 - Deactivated | DOUT#.STATE = 0, voltage removed on I/O pin |
| 1 - Activated | DOUT#.STATE = 1, voltage applied on I/O pin |
Examples
Usage
When DOUT#.SOURCE = 0 (user) then the corresponding DOUT#.STATEU can be set to drive the output at the I/O pin.
Code
--> DOUT1.SOURCE 0 //user --> DOUT1.STATEU 0 --> DOUT1.STATE 0 --> DOUT1.STATEU 1 --> DOUT1.STATE 1
Context
See Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
|
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | N/A |
| Data Type | Integer |
| See Also | |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
21050 |
1 |
21050 (0x523a) |
DOUT1.STATEU |
Unsigned8 |
Read/Write |
Yes |
|
21051 |
1 |
21051 (0x523b) |
DOUT2.STATEU |
Unsigned8 |
Read/Write |
Yes |
|
21052 |
1 |
21052 (0x523c) |
DOUT3.STATEU |
Unsigned8 |
Read/Write |
Yes |
|
21053 |
1 |
21053 (0x523d) |
DOUT4.STATEU |
Unsigned8 |
Read/Write |
Yes |
|
21054 |
1 |
21054 (0x523e) |
DOUT5.STATEU |
Unsigned8 |
Read/Write |
Yes |
|
21055 |
1 |
21055 (0x523f) |
DOUT6.STATEU |
Unsigned8 |
Read/Write |
Yes |
|
21056 |
1 |
21056 (0x5240) |
DOUT7.STATEU |
Unsigned8 |
Read/Write |
Yes |
|
21057 |
1 |
21057 (0x5241) |
DOUT8.STATEU |
Unsigned8 |
Read/Write |
Yes |
|
21058 |
1 |
21058 (0x5242) |
DOUT9.STATEU |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DOUT1.STATEU |
21050 |
Unsigned8 |
Read/Write |
- |
|
DOUT2.STATEU |
21051 |
Unsigned8 |
Read/Write |
- |
|
DOUT3.STATEU |
21052 |
Unsigned8 |
Read/Write |
- |
|
DOUT4.STATEU |
21053 |
Unsigned8 |
Read/Write |
- |
|
DOUT5.STATEU |
21054 |
Unsigned8 |
Read/Write |
- |
|
DOUT6.STATEU |
21055 |
Unsigned8 |
Read/Write |
- |
|
DOUT7.STATEU |
21056 |
Unsigned8 |
Read/Write |
- |
|
DOUT8.STATEU |
21057 |
Unsigned8 |
Read/Write |
- |
|
DOUT9.STATEU |
21058 |
Unsigned8 |
Read/Write |
- |