DRV.NVCLEAR
Description
The DRV.NCLEAR command erases the stored NV parameters. The current parameter settings are unchanged after executing this command. If an unexpected issue with the drive parameters occurs and the drive does not boot properly, the DRV.NCLEAR command can be used to recover. All parameters will use default values if the drive is power cycled or DRV.NVLOAD is executed after executing this command.
An argument is needed to confirm that it is intentional to delete the parameters: 0xAABBCCDD.
Examples
-->DRV.NVCLEAR 0xAABBCCDD
-->
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-09-02-000 |
General Information
| Type | Command |
| Units | N.A |
| Range | N/A |
| Default Value | N/A |
|
Data Type |
Integer |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
DRV.NVCLEAR |
3000h |
0eh |
Unsigned32 |
- |
- |
Write only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2022 |
1 |
2022 (0x7e6) |
DRV.NVCLEAR |
Unsigned32 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DRV.NVCLEAR |
2022 |
Unsigned32 |
Read/Write |
- |