DRV.NVDUMP
Description
Returns the parameters and values that are currently stored in NV memory. These are the values that are restored when the drive reboots or when executing DRV.NVLOAD .
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-09-02-000 |
General Information
| Type | Read Only |
| Units | N.A |
| Range | N/A |
| Default Value | N/A |
|
Data Type |
String |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.