ECAT.ENEMCY
Description
This parameter is used to enable or disable the EtherCAT emergency messaging.
| Value | Description |
|---|---|
| 0 | Disabled |
| 1 | Enabled |
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
1 |
|
Data Type |
Integer |
Variants Supported
EtherCAT drives: AKD2G-SPE
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
ECAT.ENEMCY |
4300h |
08h |
Unsigned8 |
- |
- |
Read/Write |
No |