ECAT.MISSEDRXCOUNT

Description

This command can read the actual counter value of the SM2 event missed counter. This is checked against the limit set by the object 0x10F1 sub 2 (ECAT.MAXSYNCERROR). Fault F7011 is thrown if this counter reaches the limit and theEtherCAT communication state will change to SAFE-OP with an AL status code 0x34.

Versions

Action Version Notes
Implemented 02-10-04-000  

General Information

Type

ReadOnly

Units

N/A

Range

0 to 65532

Default Value

9

Data Type

Integer

Stored in Non-Volatile Memory

No

Variants Supported

EtherCAT variants: AKD2G-SPE