ECAT.RXIRQTIME
Description
This parameter allows viewing and recording of the Distributed Clock (DC) time when the drive received the output packet (RxPDO). This is the same time as the SM2 event.
Context
See EtherCAT Drive Synchronization.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-07-04-000 |
General Information
|
Type |
Read Only |
|
Units |
ns |
|
Range |
0 to 4,294,967,295 ns |
|
Default Value |
N/A |
|
Data Type |
Integer |
| See Also | ECAT.RXDONETIME, ECAT.POSLOOPTIME, ECAT.TXDONETIME, ECAT.SYNC0TIME |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
EtherCAT variants: AKD2G-SPE