EEO#.POUT

Description

EEO#.POUT is used in conjunction with EEO#.PIN to set the gain of the EEO position going to the EEO Generator. The maximum value of EEO#.PIN / EEO#.POUT is 32.

Versions

Action Version Notes
Implemented 02-07-00-000

General Information

Type Read/Write
Description Sets the gear OUT of the EEO postision
Units N/A
Range 1 to 4,294,967,295
Default Value 1
Data Type Integer
See Also EEO#.PIN
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

EEO1.POUT

4600h

09h

Unsigned32

-

-

Read/Write

No

EEO2.POUT

4601h

09h

Unsigned32

-

-

Read/Write

No

EEO3.POUT

4603h

09h

Unsigned32

-

-

Read/Write

No

EEO4.POUT

4606h

09h

Unsigned32

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

32050

1

32050 (0x7d32)

EEO1.POUT

Unsigned32

Read/Write

Yes

32051

1

32051 (0x7d33)

EEO2.POUT

Unsigned32

Read/Write

Yes

32052

1

32052 (0x7d34)

EEO3.POUT

Unsigned32

Read/Write

Yes

32053

1

32053 (0x7d35)

EEO4.POUT

Unsigned32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

EEO1.POUT

32050

Unsigned32

Read/Write

-

EEO2.POUT

32051

Unsigned32

Read/Write

-

EEO3.POUT

32052

Unsigned32

Read/Write

-

EEO4.POUT

32053

Unsigned32

Read/Write

-