EIP.MISSEDPACKETCOUNT

Description

The internal counter used to trigger F7005 Cyclic Setpoints Missing fault. The counter increments by 3 on every missed cyclic packet and decrements by 1 when a packet is received.

Examples

The following chart provides an example of how the fault counter behaves using the default threshold of 9:

Fieldbus Cycle

Packet Received

Counter

Faulted

0

Yes

0

No

1

Yes

0

No

2

No

3

No

3

Yes

2

No

4

Yes

1

No

5

No

4

No

6

No

7

No

7

Yes

6

No

8

No

9

Yes

9

Yes

8

Yes

10

Yes

7

Yes

11

Yes

6

Yes

Context

EIP.PACKETMISSTHRESHOLD

Versions

Action Version Notes
Implemented 02-10-04-000

General Information

Type

Read/Write

Units

N/A

Range

0 (disabled) to 216

Default Value

9

Data Type

Integer

Stored in Non-Volatile Memory

No

Variants Supported

EtherNet/IP drives: AKD2G-SPI

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

3903

1

3903 (0xf3f)

EIP.MISSEDPACKETCOUNT

Unsigned16

Read Only

Yes