FB#.SCALED.ZERO
Description
This command updates FB#.SCALED.P to 0 by changing FB#.SCALED.OFFSET to the negative value of FB#.SCALED.P before it is zeroed.
Example
Code
-->FB1.SCALED.OFFSET
1999.999 [deg]
-->FB1.SCALED.P
417447.831 [deg]
-->FB1.SCALED.ZERO
-->FB1.SCALED.OFFSET
-415447.804 [deg]
-->FB1.SCALED.P
0.000 [deg]
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-10-02-000 |
General Information
|
Type |
ReadOnly |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
|
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.