FB#.STOREMULTITURN.ENABLE
Description
This keyword enables or disables the store multiturn feature.
To prevent rollovers, set FB#.STOREMULTITURN.ENABLE = 1. Whenever the drive is power cycled after passing multiturn rollovers, the drive will keep track of the rollovers and retain the correct position.
| Enabled | |
|---|---|
| 0 (default) | Disabled |
| 1 | Enabled |
Context
See Store Multiturn
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-08-03-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0, 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
FB1.STOREMULTITURN.ENABLE |
3500h |
0fh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
FB2.STOREMULTITURN.ENABLE |
3501h |
0fh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
FB3.STOREMULTITURN.ENABLE |
3502h |
0fh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
FB4.STOREMULTITURN.ENABLE |
3503h |
0fh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
FB5.STOREMULTITURN.ENABLE |
3504h |
0fh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
30460 |
1 |
30460 (0x76fc) |
FB1.STOREMULTITURN.ENABLE |
Unsigned8 |
Read/Write |
Yes |
|
30461 |
1 |
30461 (0x76fd) |
FB2.STOREMULTITURN.ENABLE |
Unsigned8 |
Read/Write |
Yes |
|
30462 |
1 |
30462 (0x76fe) |
FB3.STOREMULTITURN.ENABLE |
Unsigned8 |
Read/Write |
Yes |
|
30463 |
1 |
30463 (0x76ff) |
FB4.STOREMULTITURN.ENABLE |
Unsigned8 |
Read/Write |
Yes |
|
30464 |
1 |
30464 (0x7700) |
FB5.STOREMULTITURN.ENABLE |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
FB1.STOREMULTITURN.ENABLE |
30460 |
Unsigned8 |
Read/Write |
- |
|
FB2.STOREMULTITURN.ENABLE |
30461 |
Unsigned8 |
Read/Write |
- |
|
FB3.STOREMULTITURN.ENABLE |
30462 |
Unsigned8 |
Read/Write |
- |
|
FB4.STOREMULTITURN.ENABLE |
30463 |
Unsigned8 |
Read/Write |
- |
|
FB5.STOREMULTITURN.ENABLE |
30464 |
Unsigned8 |
Read/Write |
- |