FB#.CALTHRESHRES

Description

FB#.CALTHRESHRES sets the velocity threshold at which the auto-calibration function continuously updates error correction for Resolver encoders in electrical Hz.

Context

Only used for resolver feedbacks. See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Electrical Hz

Range

0Hz to 65535Hz

Default Value

3 Hz

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.CALTHRESHRES

3500h

07h

Unsigned16

-

-

Read/Write

No

FB2.CALTHRESHRES

3501h

07h

Unsigned16

-

-

Read/Write

No

FB3.CALTHRESHRES

3502h

07h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30440

1

30440 (0x76e8)

FB1.CALTHRESHRES

Unsigned16

Read/Write

Yes

30441

1

30441 (0x76e9)

FB2.CALTHRESHRES

Unsigned16

Read/Write

Yes

30442

1

30442 (0x76ea)

FB3.CALTHRESHRES

Unsigned16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.CALTHRESHRES

30440

Unsigned16

Read/Write

-

FB2.CALTHRESHRES

30441

Unsigned16

Read/Write

-

FB3.CALTHRESHRES

30442

Unsigned16

Read/Write

-