FB#.HALLSTATE

Description

FB#.HALLSTATE reads the Hall switch values (encoder feedback only).

The value is the sum of the three hall bit states, where FB#.HALLSTATE = Hall U + Hall V + Hall W. If the hall is not active, it returns 0. When a hall is active, each hall contributes the following value to the sum:

  • Hall W = 1
  • Hall V = 2
  • Hall U = 4
Value Hall W Hall V Hall U
1 - -
2 - -
3 -
4 - -
5 -
6 -

The following sequences indicate the direction of rotation.

Sequence Direction
1,5,4,6,2,3,1 Positive
1,3,2,6,4,5,1 Negative

These commands are not recordable on FB1 and FB2.

For recording on FB1 and FB2, see FB#.MONITOR#.SOURCE and FB#.MONITOR#.DATA.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Terminal: Binary

Scope: N/A

Range

Terminal: See description above

Scope: 1 to 6

Default Value

N/A

Data Type

Terminal: String

Scope: Integer

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.HALLSTATE

3500h

1ah

Unsigned8

-

-

Read only

No

FB2.HALLSTATE

3501h

1ah

Unsigned8

-

-

Read only

No

FB3.HALLSTATE

3502h

1ah

Unsigned8

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30060

1

30060 (0x756c)

FB1.HALLSTATE

Unsigned8

Read Only

Yes

30061

1

30061 (0x756d)

FB2.HALLSTATE

Unsigned8

Read Only

Yes

30062

1

30062 (0x756e)

FB3.HALLSTATE

Unsigned8

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.HALLSTATE

30060

Unsigned8

Read Only

-

FB2.HALLSTATE

30061

Unsigned8

Read Only

-

FB3.HALLSTATE

30062

Unsigned8

Read Only

-

Related Topics

FB#.MONITOR#.DATA

FB#.MONITOR#.SOURCE