FB#.POSLOWPASS
Description
FB#.POSLOWPASS configures an averaging filter that is run inside the feedback device at a high data rate. This is used to lower measured position noise and help prevent aliasing from the feedback sampling rate to the drive.
-
- Currently only SFD-M supports this feature. FB#.POSLOWPASS is only implemented when FB#.SELECT = 47 (SFD-M). It is ignored for other values of FB#.SELECT.
The following table lists the supported filter values.
|
Value |
Notes |
|---|---|
|
0 |
No Filter |
|
1 |
4 kHz low-pass filter |
|
2 |
8 kHz low-pass filter |
Context
See Feedback # View.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-14-00-000 | — |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 2 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
FB1.POSLOWPASS |
3500h |
21h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
FB2.POSLOWPASS |
3501h |
21h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
30880 |
1 |
30880 (0x78a0) |
FB1.POSLOWPASS |
Unsigned8 |
Read/Write |
Yes |
|
30881 |
1 |
30881 (0x78a1) |
FB2.POSLOWPASS |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
FB1.POSLOWPASS |
30880 |
Unsigned8 |
Read/Write |
- |
|
FB2.POSLOWPASS |
30881 |
Unsigned8 |
Read/Write |
- |