FB#.SSITYPE

Description

FB#.SSITYPE sets the type of SSI device used for position feedbacks. The SSI protocol is flexible and compatible with different feedback models using different implementations. The protocols may differ in the data format of the serial position bits. They also may contain special configuration and flag bits.

FB#.SSITYPE is used when FB#.SELECT = 36 (SSI). It is ignored for other values of FB#.SELECT.

The following table lists the supported SSI types with protocol details and example manufacturers and models.

Value Protocol Models Notes
0 Binary position bits only Netzer DS-25-SF-S0  
1 Grey code position bits only Hengstler AD34/1217AF.0NSC0:5942  
2

1 status bit

Grey code position bits

3 flag bits

1 zero bit

Gurley VP12S08A2CN ‘Initializing move’ required before position values from FB#.P are valid and will cause position jump on completion. See encoder datasheet for details.

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-06-03-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 2

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.SSITYPE

3500h

12h

Unsigned8

-

-

Read/Write

No

FB2.SSITYPE

3501h

12h

Unsigned8

-

-

Read/Write

No

FB3.SSITYPE

3502h

12h

Unsigned8

-

-

Read/Write

No

FB4.SSITYPE

3503h

12h

Unsigned8

-

-

Read/Write

No

FB5.SSITYPE

3504h

12h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30560

1

30560 (0x7760)

FB1.SSITYPE

Unsigned8

Read/Write

Yes

30561

1

30561 (0x7761)

FB2.SSITYPE

Unsigned8

Read/Write

Yes

30562

1

30562 (0x7762)

FB3.SSITYPE

Unsigned8

Read/Write

Yes

30563

1

30563 (0x7763)

FB4.SSITYPE

Unsigned8

Read/Write

Yes

30564

1

30564 (0x7764)

FB5.SSITYPE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.SSITYPE

30560

Unsigned8

Read/Write

-

FB2.SSITYPE

30561

Unsigned8

Read/Write

-

FB3.SSITYPE

30562

Unsigned8

Read/Write

-

FB4.SSITYPE

30563

Unsigned8

Read/Write

-

FB5.SSITYPE

30564

Unsigned8

Read/Write

-