GANTRY.PL.ERRTTHRESH

Description

This parameter sets a time threshold the maximum position error (GANTRY.PL.ERRFTHRESH) must exceed before a Gantry Position Error fault is thrown.

Mechanics can introduce a certain amount of error when the system is disabled and "relaxes". The error in the relaxed state may end up being greater than the maximum position error, which causes a fault to be thrown when the gantry is re-enabled. This time threshold allows for ignoring the error. Setting this command to a non-zero value allows the system to enable and correct itself before throwing a fault.

A fault is immediately thrown when GANTRY.PL.ERR exceeds maximum position error if this parameter is set to 0.

Versions

Action Version Notes
Implemented 02-07-00-000  

General Information

Type Parameter
Description Sets the time threshold a gantry position error must persist before a fault is thrown.
Units Seconds
Range 0.000 to 10.000
Default Value 1.000
Data Type Float
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

GANTRY.PL.ERRTTHRESH

300eh

06h

Unsigned16

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

3005

1

3005 (0xbbd)

GANTRY.PL.ERRTTHRESH

Unsigned16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

GANTRY.PL.ERRTTHRESH

3005

Float

Read/Write

-

Related Topics

Electronic Gearing