HW.FANSPEED#

Description

This parameter returns the current speed of the fan that provides cooling for the specified power board.

Examples

Usage

The parameter value can be used to track the fan speed as it changes based on power board temperature.



At powerup, the drive runs the fan at full speed for a brief duration to ensure correct operation. It then ramps the fan down to normal operating speed. After powerup, the drive adjusts the fan speed as the power board temperature changes during drive operation.

Code

--> HW.FANSPEED1
1754.611731 [rpm]

Context

For more information on fan operation, see Power View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units rpm
Range N/A
Default Value N/A
Data Type Float
See Also  

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

HW.FANSPEED1

301dh

01h

Signed32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2900

1

2900 (0xb54)

HW.FANSPEED1

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

HW.FANSPEED1

2900

Float

Read Only

-