IP.PROTOCOL
This parameter is used to determine the protocol used to connect to the drive.
Examples
Usage
- Use Telnet to connect to the drive (default).
- Use both SSH and Telnet to connect to the drive.
-
- SSH is not fully supported at this time.
Code
Get help on IP.PROTOCOL and then set SSH and Telnet as the allowed protocols to connect to the drive.
--> DRV.HELP IP.PROTOCOL
Help for IP.Protocol [Integer] [NV] [ReadWrite] [Enum] Minval = 0 Maxval = 1 Default = 0 Actual value = 0 (Telnet only) Values = 0 (Telnet only), 1 (Both SSH and Telnet)
--> IP.PROTOCOL 1
Context
For more information on IP configuration for telnet, see Finding and Connecting to a Device.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-03-03-000 |
|
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | 0 |
| Data Type | Integer |
| See Also | IP.ADDRESS, IP.SUBNET, IP.GATEWAY IP.RESET |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
IP.PROTOCOL |
3013h |
05h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2204 |
1 |
2204 (0x89c) |
IP.PROTOCOL |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
IP.PROTOCOL |
2204 |
Unsigned8 |
Read/Write |
- |