MODBUS.ERRORCOUNT
Description
The number of errors logged since the drive powered up or the error log was cleared with MODBUS.CLRERRORS.
Example
The following shows the error count changing after the error log is cleared.
-->MODBUS.ERRORCOUNT 2 -->MODBUS.ERRORS (39d:21h:30m:48s) Write 40002: Modbus error code 34 (Command Error), Error 7 (Command is read-only)
(39d:21h:45m:22s) Read 45001: Modbus error code 38 (Length Invalid) -->MODBUS.CLRERRORS -->MODBUS.ERRORCOUNT 0 -->
Context
For more information, see Modbus Errors.
Versions
| Action | Version | Notes |
|---|---|---|
|
Implemented |
02-05-00-000 |
General Information
|
Type |
Read Only Parameter |
|
Units |
N/A |
|
Range |
0 to 65535 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non-Volatile Memory |
No |
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
MODBUS.ERRORCOUNT |
3014h |
07h |
Unsigned16 |
- |
- |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
3704 |
1 |
3704 (0xe78) |
MODBUS.ERRORCOUNT |
Unsigned16 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
MODBUS.ERRORCOUNT |
3704 |
Unsigned16 |
Read Only |
- |