MODBUS.INFO
Description
DRV.INFO returns information about the current Modbus connections to the drive.
If no Modbus connections are used the count is 0.
-->MODBUS.INFO Connection count: 0 -->
If one connection to the drive is established the following information is provided. The IP address displays the port and the device that is connected to the AKD2Gdrive.
-->MODBUS.INFO Connection count: 1 Connection 1 address: 192.168.1.20:48855 Connection 1 read count: 1 Connection 1 write count: 0 Connection 1 connect time: 15s -->
Each connection is assigned a unique number when the connection is established and the number is static. The following example provides the connection information with two active connections and four connections that were previously opened and then closed.
-->MODBUS.INFO Connection count: 2 Connection 6 address: 10.8.232.205:46302 Connection 6 read count: 2 Connection 6 write count: 0 Connection 6 connect time: 38s Connection 2 address: 10.8.232.205:47326 Connection 2 read count: 1 Connection 2 write count: 0 Connection 2 connect time: 2s -->
Context
For more information, see High Message Rates.
Versions
| Action | Version | Notes |
|---|---|---|
|
Implemented |
02-05-00-000 |
General Information
|
Type |
Info Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
String |
|
See Also |
N/A |
|
Stored in Non-Volatile Memory |
No |