MODBUS.LIST
Description
MODBUS.LIST prints a list of all the parameters that are mapped using MODBUS.MAP .
Each row provides the parameter name and additional information about that parameter when accessed using Modbus.
| Column |
Descriptions and expected values |
|---|---|
|
1 |
Parameter name. |
|
2 |
Signed: Integer that can be positive or negative. Unsigned: Integer that is only positive. Float: A number with a fractional part. The number read or written over Modbus is an integer that is 1000 times the value as displayed in WorkBench. For example, 12.034 in WorkBench is 12034 over Modbus. ActionCommand: Triggers the action when the value changes from 0 to any non-zero value. |
|
3 |
The minimum width of the parameter when accessed over Modbus. 16-bit – These parameters only require one Modbus register. 32-bit – These parameters require two consecutive 16-bit Modbus registers. |
|
4 |
ReadWrite or ReadOnly Writing to a read only parameter can generate a Modbus error depending on the setting MODBUS.ERRORMODE. |
Examples
Type the command to view the current mapping for all the Modbus addresses.
-->MODBUS.LIST AIN1.DEADBAND,Float,16-bit,ReadWrite AIN1.DEADBANDMODE,Unsigned,16-bit,ReadWrite AIN1.OFFSET,Float,16-bit,ReadWrite AIN1.VALUE,Float,16-bit,ReadOnly AIN2.DEADBAND,Float,16-bit,ReadWrite AIN2.DEADBANDMODE,Unsigned,16-bit,ReadWrite AIN2.OFFSET,Float,16-bit,ReadWrite AIN2.VALUE,Float,16-bit,ReadOnly … -->
Context
For more information, see Editing the Map.
Versions
| Action | Version | Notes |
|---|---|---|
|
Implemented |
02-05-00-000 |
General Information
|
Type |
Info Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
|
|
Stored in Non-Volatile Memory |
No |