PROFINET.ENISOWARNING

Description

This parameter allows warning 7012 (IRT not configured correctly and selected telegram requires synchronization in PLC) to be disbaled. If for some reason the application does not require isochronous mode under conditions the drive would normally recommend it be enabled, this can be used to force the warning to become inactive.

Context

See warning W7012.

Versions

Action Version Notes
Implemented 02-06-03-000  

General Information

Type Read/Write
Units N/A
Range 0 or 1
Default Value 1
Data Type Integer
Stored in Non-Volatile Memory Yes

Variants Supported

PROFINET drives: AKD2G-SPP

Industrial Ethernet Information

PROFINET

Parameter

PNU

Data Type

Access

Units

PROFINET.ENISOWARNING

3303

Unsigned8

Read/Write

-