REGEN.TEMP

Description

This parameter returns the measured temperature of the power module for the regen resistor.

Versions

Action

Version

Notes

Implemented

02-07-03-000

General Information

Type

Read Only

Units

Deg C

Range

N/A

Default Value

N/A

Data Type

Float

See Also

 

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

REGEN.TEMP

3007h

0bh

Unsigned8

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2410

1

2410 (0x96a)

REGEN.TEMP

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.TEMP

2410

Float

Read Only

-