REGEN.TESTTO

Description

This command is used to configure the timeout expected by the regen self-test feature. See REGEN.TEST for more info on how this timeout is used.

Versions

Action

Version

Notes

Implemented

02-07-03-000

General Information

Type

Read/Write

Units

Milliseconds

Range

1 to 4000

Default Value

1000

Data Type

Integer

See Also

REGEN.TEST

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

REGEN.TESTTO

3007h

09h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2408

1

2408 (0x968)

REGEN.TESTTO

Unsigned16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.TESTTO

2408

Unsigned16

Read/Write

-