REGEN.TESTVTHRESH

Description

This command is used to configure the timeout expected by the regen self-test feature. See REGEN.TEST for more info on how this timeout is used.

Versions

Action

Version

Notes

Implemented

02-07-03-000

General Information

Type

Read/Write

Units

Percent (%)

Range

60 to 99

Default Value

80

Data Type

Integer

See Also

REGEN.TEST

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

REGEN.TESTVTHRESH

3007h

0ah

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2409

1

2409 (0x969)

REGEN.TESTVTHRESH

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.TESTVTHRESH

2409

Unsigned8

Read/Write

-