REGEN.UTFTHRESH
Description
This parameter returns the over temperature warning threshold of the power circuit for the regen resistor. The value depends on the drive model. It is programmed in the drive and cannot be changed.
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-08-01-000 |
|
General Information
|
Type |
Read Only |
|
Units |
Deg C |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Float |
|
See Also |
|
|
Stored in Non-Volatile Memory |
|
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
REGEN.UTFTHRESH |
3007h |
0eh |
Unsigned8 |
- |
- |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2413 |
1 |
2413 (0x96d) |
REGEN.UTFTHRESH |
Signed32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
REGEN.UTFTHRESH |
2413 |
Float |
Read Only |
- |