SD.LOGEN
Description
This parameter turns on logging to the SD card.
Example
Usage
This parameter is meant to be used as part of drive NV parameters to always log to the SD card. By default, the drive creates log messages stored in the flash. In addition, if it is desired, the user can also store these log messages to the SD card. Log files are automatically rolled over when they reach 1M in size, and they are stored on the SD card, at /akd2g_drives/<drive-name>/log_files.
Code
-->DRV.HELP SD.LOGEN
Help for: SD.LOGEN [Integer] [NV] [ReadWrite]
Minval = 0
Maxval = 1
Default = 0
Actual value = 0
Extended timeout = 10 [s]
-->SD.LOGEN 1
-->SD.LOGEN 0
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-04-01-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0, 1 |
|
Default Value |
0 |
|
Data Type |
N/A |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
SD.LOGEN |
3010h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
3400 |
1 |
3400 (0xd48) |
SD.LOGEN |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
SD.LOGEN |
3400 |
Unsigned8 |
Read/Write |
- |