SD.STATUS
Description
This parameter checks the status of the SD card.
Example
Usage
It is used to check if there is an SD card inside the drive slot. It also reports if the SD card is write-protected.
Code
-->SD.STATUS 0 (Ready) -->SD.STATUS 2 (Not Inserted) -->SD.STATUS 1 (Read Only)
Context
See LCD Display for using the SD card to perform backup and restore operations.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Stored in Non-Volatile Memory |
N/A |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
SD.STATUS |
3010h |
02h |
Unsigned8 |
- |
- |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
3401 |
1 |
3401 (0xd49) |
SD.STATUS |
Unsigned8 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
SD.STATUS |
3401 |
Unsigned8 |
Read Only |
- |